Keysight 89600 VSA .NET API
ActiveSlotsAutoDetected Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > Csirs Class : ActiveSlotsAutoDetected Property


Glossary Item Box

Gets or sets a value indicating whether the active slots are auto detected..

Syntax

Visual Basic (Declaration) 
Public Overridable Property ActiveSlotsAutoDetected As Boolean
C# 
public virtual bool ActiveSlotsAutoDetected {get; set;}
C++/CLI 
public:
virtual property bool ActiveSlotsAutoDetected {
   bool get();
   void set (    bool value);
}

Property Value

The default value is false.

Remarks

When this value is true, the active slots are auto detected; when this value is false, the user configured slots are assumed to be always active.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 28.40

See Also