Keysight 89600 VSA .NET API
Csirs Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : Csirs Class

Glossary Item Box

The following tables list the members exposed by Csirs.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyActiveSlotsAutoDetectedGets or sets a value indicating whether the active slots are auto detected..  28.40
Public PropertyAntennaDetectionThresholdGets or sets a value indicating the power threshold (in dB) used for detecting whether an antenna port is active on an input channel for this CSI-RS.  —
Public PropertyAntennaPortGets or sets a value indicating which CSI-RS antenna port to be analyzed.  —
Public PropertyAntennaPortNumberGets or sets the CSI-RS antenna port number.  —
Public PropertyAreResourceElementsUsedForPdschGets or sets a value indicating whether the CSI-RS resource elements can be used by any PDSCH or not.  26.00
Public PropertyBwpIdGets or sets BWP Id  24.20
Public PropertyCdmTypeGets or sets the CSI-RS CDM Type.  —
Public PropertyDensityGets or sets the CSI-RS density in frequency domain.  —
Public PropertyFlexibleSymbolsGets or sets the flexible symbols to be used in the slot format.  —
Public PropertyIsCsirsEnabledGets or sets a value indicating whether the physical channel is marked as enabled.  —
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyIsIncludedInRmsEvmGets or sets a value indicating whether CsiRs is included in RMS EVM calculation/>.  24.20
Public PropertyIsZeroPowerEnabledGets or sets a value indicating whether the CSI-RS is zero power or not.  —
Public PropertyL0SymbolIndexGets or sets a value indicating the L0 start symbol index in a slot used by this physical channel.  —
Public PropertyL1SymbolIndexGets or sets a value indicating the L1 start symbol index in a slot used by this physical channel.  —
Public PropertyNidGets or sets CSI-RS Scrambling Id  —
Public PropertyPeriodicityGets or sets a value indicating the CSI-RS periodicity in slots. Default value is 20 slots.  28.40
Public PropertyPeriodicityEnabledGets or sets a value indicating whether the CSI-RS periodicity is enabled.  28.40
Public PropertyPowerBoostingGets or sets a value indicating the relative power boosting (in dB) of this physical channel.  —
Public PropertyRBNumberGets or sets a value indicating the number of resource blocks assigned to the physical channel.  —
Public PropertyRBOffsetGets or sets a value indicating the start index of resource block assigned to the physical channel.  —
Public PropertySfiGets or sets the slot format indicator used for this CSI-RS physical channel.  —
Public PropertySlotOffsetGets or sets a value indicating the CSI-RS slot offset within the Periodicity.  28.40
Public PropertyTableRowIndexGets or sets the row index of table 7.4.1.5.3-1 in 38.211  —
Public PropertyTableRowIndexEnabledGets or sets a value indicating whether using the row index of 7.4.1.5.3-1 in 38.211 to configure the CSI-RS.  25.40
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetAllocatedSlotIndexesGets the set of slot indexes allocated for this physical channel.  —
Public MethodGetFrequencyDomainAllocationGets the frequency domain allocation.  25.40
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodGetSfiDescriptionGets the slot format indicator detailed description indicating the symbol directions.  —
Public MethodGetSfiSymbolDirectionsGets the slot format indicator symbol directions.  —
Public MethodGetValidSfiValuesGet the valid slot format indicator values.  —
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodSetAllocatedSlotIndexesOverloaded. Sets a single contiguous set of slots to be allocated for this physical channel.  —
Public MethodSetFrequencyDomainAllocationSets frequency domain allocation from specification 38.211 clause 7.4.1.5.3 CSI-RS-ResourceMapping.  25.40
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also