Keysight 89600 VSA .NET API
AntennaDetectionThreshold Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > Csirs Class : AntennaDetectionThreshold Property


Glossary Item Box

Gets or sets a value indicating the power threshold (in dB) used for detecting whether an antenna port is active on an input channel for this CSI-RS.

Syntax

Visual Basic (Declaration) 
Public Overridable Property AntennaDetectionThreshold As Double
C# 
public virtual double AntennaDetectionThreshold {get; set;}
C++/CLI 
public:
virtual property double AntennaDetectionThreshold {
   double get();
   void set (    double value);
}

Property Value

The default value is -36.0.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also