Keysight 89600 VSA .NET API
AntennaPort Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > Csirs Class : AntennaPort Property


Glossary Item Box

Gets or sets a value indicating which CSI-RS antenna port to be analyzed.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property AntennaPort As Integer
C# 
public abstract int AntennaPort {get; set;}
C++/CLI 
public:
abstract property int AntennaPort {
   int get();
   void set (    int value);
}

Property Value

Default value is 3000. Valid range is from 3000 to 3031.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also