| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property FlexibleSymbols As Integer | |
| C# | |
|---|---|
public abstract int FlexibleSymbols {get; set;} | |
Property Value
The default is 0, indicating no "Flexible" symbols should be allocated to this physical channel.This property helps define the set of symbols reserved for this CSI-RS physical channel. This value represents a bitmap to indicate which "Flexible" symbols from the Sfi should be available to this CSI-RS physical channel (in every slot). This is applied in coordination with Sfi.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)