Keysight 89600 VSA .NET API
IsZeroPowerEnabled Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > Csirs Class : IsZeroPowerEnabled Property


Glossary Item Box

Gets or sets a value indicating whether the CSI-RS is zero power or not.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property IsZeroPowerEnabled As Boolean
C# 
public abstract bool IsZeroPowerEnabled {get; set;}
C++/CLI 
public:
abstract property bool IsZeroPowerEnabled {
   bool get();
   void set (    bool value);
}

Remarks

Default value is false.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also