Keysight 89600 VSA .NET API
Nid Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > Csirs Class : Nid Property


Glossary Item Box

Gets or sets CSI-RS Scrambling Id

Syntax

Visual Basic (Declaration) 
Public MustOverride Property Nid As Integer
C# 
public abstract int Nid {get; set;}
C++/CLI 
public:
abstract property int Nid {
   int get();
   void set (    int value);
}

Remarks

Default value is 0. Range of value is 0 through 65535.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also