Keysight 89600 VSA .NET API
SlotOffset Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > Csirs Class : SlotOffset Property


Glossary Item Box

Gets or sets a value indicating the CSI-RS slot offset within the Periodicity.

Syntax

Visual Basic (Declaration) 
Public Overridable Property SlotOffset As Integer
C# 
public virtual int SlotOffset {get; set;}
C++/CLI 
public:
virtual property int SlotOffset {
   int get();
   void set (    int value);
}

Remarks

Default value is 0. Range is from 0 to (Periodicity -1).

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 28.40

See Also