Keysight 89600 VSA .NET API
DmrsAddPosition Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : DmrsAddPosition Enumeration


Glossary Item Box

Enum values indicating the DMRS-add-pos type

Syntax

Visual Basic (Declaration) 
Public Enum DmrsAddPosition 
   Inherits System.Enum
C# 
public enum DmrsAddPosition : System.Enum 
C++/CLI 
public enum class DmrsAddPosition : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
Pos0DMRS-add-pos is Type 0.—
Pos1DMRS-add-pos is Type 1.—
Pos2DMRS-add-pos is Type 2.—
Pos3DMRS-add-pos is Type 3.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 23.00

See Also