Keysight 89600 VSA .NET API
DmrsAddPos Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > Pusch Class : DmrsAddPos Property


Glossary Item Box

Gets or sets a value indicating the additional DMRS positions for this physical channel.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property DmrsAddPos As DmrsAddPosition
C# 
public abstract DmrsAddPosition DmrsAddPos {get; set;}
C++/CLI 
public:
abstract property DmrsAddPosition DmrsAddPos {
   DmrsAddPosition get();
   void set (    DmrsAddPosition value);
}

Property Value

Default value is DmrsAddPosition.Pos0.

Remarks

Refer to 6.4.1.1.3 of 38.211 for more details

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also