Keysight 89600 VSA .NET API
DmrsInitValueDefinition Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : DmrsInitValueDefinition Enumeration


Glossary Item Box

Enum values indicating the specification interpretation to apply for DMRS sequence initialization.

Syntax

Visual Basic (Declaration) 
Public Enum DmrsInitValueDefinition 
   Inherits System.Enum
C# 
public enum DmrsInitValueDefinition : System.Enum 
C++/CLI 
public enum class DmrsInitValueDefinition : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
CinitDMRS sequence generation is initialized with the c_init value.—
Custom1DMRS sequence generation is initialized according to Custom1 value.—
NRDMRS sequence generation is initialized according to the 3GPP-NR standard version 15.0.0 (2017-12).—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Remarks

NOTE: These options are provided to handle special-case interpretation of DMRS initialization. In most cases NR should be used.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 23.00

See Also