Keysight 89600 VSA .NET API
DmrsMaxLength Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : DmrsMaxLength Enumeration


Glossary Item Box

Enum values indicating maximum possible length of DMRS for physical channel

Syntax

Visual Basic (Declaration) 
Public Enum DmrsMaxLength 
   Inherits System.Enum
C# 
public enum DmrsMaxLength : System.Enum 
C++/CLI 
public enum class DmrsMaxLength : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
OneDMRS Max Length is one symbol.—
TwoDMRS Max Length is two symbols.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 23.00

See Also