Keysight 89600 VSA .NET API
DmrsMaxLength Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > Pusch Class : DmrsMaxLength Property


Glossary Item Box

Gets or sets a value indicating the PUSCH DMRS maximum length.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property DmrsMaxLength As DmrsMaxLength
C# 
public abstract DmrsMaxLength DmrsMaxLength {get; set;}
C++/CLI 
public:
abstract property DmrsMaxLength DmrsMaxLength {
   DmrsMaxLength get();
   void set (    DmrsMaxLength value);
}

Property Value

Default value is DmrsMaxLength.One.

Remarks

The DMRS Max Length will limit DmrsDuration

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also