Keysight 89600 VSA .NET API
EqualizerTrainingSignalBasis Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : EqualizerTrainingSignalBasis Enumeration


Glossary Item Box

Enum values indicating the Equalizer Training signal basis.

Syntax

Visual Basic (Declaration) 
Public Enum EqualizerTrainingSignalBasis 
   Inherits System.Enum
C# 
public enum EqualizerTrainingSignalBasis : System.Enum 
C++/CLI 
public enum class EqualizerTrainingSignalBasis : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
NoneEqualizer Training is off.—
RSEqualizer Training is based on RS.—
RSAndDataEqualizer Training is based on the RS and Data.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Remarks

The choice determines what portion of the signal contributes to the equalizer training procedure. This affects the equalization used for demodulation, as well as the presented channel frequency response result data.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 23.00

See Also