Keysight 89600 VSA .NET API
LteCrsCarrierBandwidth Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : LteCrsCarrierBandwidth Enumeration


Glossary Item Box

Enum value indicating the LTE carrier bandwidth in RBs.

Syntax

Visual Basic (Declaration) 
Public Enum LteCrsCarrierBandwidth 
   Inherits System.Enum
C# 
public enum LteCrsCarrierBandwidth : System.Enum 
C++/CLI 
public enum class LteCrsCarrierBandwidth : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
N100The LTE carrier bandwidth is 100 RBs / 20MHz.—
N15The LTE carrier bandwidth is 15 RBs / 3MHz.—
N25The LTE carrier bandwidth is 25 RBs / 5MHz.—
N50The LTE carrier bandwidth is 50 RBs / 10MHz.—
N6The LTE carrier bandwidth is 6 RBs / 1.4MHz.—
N75The LTE carrier bandwidth is 75 RBs / 15MHz.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 25.00

See Also