Keysight 89600 VSA .NET API
LteCrsNumberOfPorts Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : LteCrsNumberOfPorts Enumeration


Glossary Item Box

Enum value indicating the number of LTE carrier CRS antenna ports.

Syntax

Visual Basic (Declaration) 
Public Enum LteCrsNumberOfPorts 
   Inherits System.Enum
C# 
public enum LteCrsNumberOfPorts : System.Enum 
C++/CLI 
public enum class LteCrsNumberOfPorts : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
FourThe number of LTE carrier CRS antenna ports is 4 (N4).—
OneThe number of LTE carrier CRS antenna ports is 1 (N1).—
TwoThe number of LTE carrier CRS antenna ports is 2 (N2).—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 25.00

See Also