| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Function Remove( _ ByVal item As LteCrsRateMatchPattern _ ) As Boolean | |
| C# | |
|---|---|
public abstract bool Remove( LteCrsRateMatchPattern item ) | |
| C++/CLI | |
|---|---|
public: abstract bool Remove( LteCrsRateMatchPattern^ item ) | |
Parameters
- item
- LteCrsRateMatchPattern to remove from the collection
Return Value
True, if the LteCrsRateMatchPattern was removed from the collection.Note the first element in the collection cannot be removed because it is the primary LteCrsRateMatchPattern.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)