Keysight 89600 VSA .NET API
AcquisitionMode Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > MeasurementExtension Class : AcquisitionMode Property


Glossary Item Box

Gets or sets the acquisition mode to use for configuring analysis.

Syntax

Visual Basic (Declaration) 
Public Overridable Property AcquisitionMode As AcquisitionMode
C# 
public virtual AcquisitionMode AcquisitionMode {get; set;}
C++/CLI 
public:
virtual property AcquisitionMode AcquisitionMode {
   AcquisitionMode get();
   void set (    AcquisitionMode value);
}

Property Value

The default value is AcquisitionMode.Normal

Remarks

This property, along with ResultLength, ResultLengthAdditionalSlots, AnalysisStartBoundary, and the settings specified in PrimaryComponentCarrier affect the amount of acquired data required for a measurement.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 24.00

See Also