| Visual Basic (Declaration) | |
|---|---|
Public Overridable Property CcdfDataSourceMode As CcdfDataSourceMode | |
| C# | |
|---|---|
public virtual CcdfDataSourceMode CcdfDataSourceMode {get; set;} | |
| C++/CLI | |
|---|---|
public: virtual property CcdfDataSourceMode CcdfDataSourceMode { CcdfDataSourceMode get(); void set ( CcdfDataSourceMode value); } | |
When deciding which time segments are included in CCDF/Time/Spectrum calculation, the resolution is one symbol. If multiple signals are allocated at the same symbol but different spectrum part, and some signals are included, some others are not included, this symbol with all spectrum components will be included in the calculation. Currently the start time of Time/CCDF/Spectrum is based on the analysis boundary of the result component carrier, so only the channel configuration of the result component carrier is used to decide which time segments are included. CcdfDataSourceMode.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 27.40