Keysight 89600 VSA .NET API
EqualizerTrainingTimeBasis Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > MeasurementExtension Class : EqualizerTrainingTimeBasis Property


Glossary Item Box

Gets or sets a value indicating what time basis interval is used for per layer equalizer training.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property EqualizerTrainingTimeBasis As EqualizerTrainingTimeBasis
C# 
public abstract EqualizerTrainingTimeBasis EqualizerTrainingTimeBasis {get; set;}
C++/CLI 
public:
abstract property EqualizerTrainingTimeBasis EqualizerTrainingTimeBasis {
   EqualizerTrainingTimeBasis get();
   void set (    EqualizerTrainingTimeBasis value);
}

Property Value

The default value is EqualizerTrainingTimeBasis.Frame

Remarks

When set to EqualizerTrainingTimeBasis.Slot, only signals within each demodulated slot contribute to the equalizer used to demodulation that slot. When set to EqualizerTrainingTimeBasis.ContiguousSlots, only signals within each demodulated contiguous slot region contribute to the equalizer used to demodulation that contiguous slot region. When set to EqualizerTrainingTimeBasis.Subframe, only signals within each demodulated subframe contribute to the equalizer used to demodulation that subframe. When set to EqualizerTrainingTimeBasis.Frame, only signals within each demodulated frame contribute to the equalizer used to demodulation that frame. When set to EqualizerTrainingTimeBasis.ResultLength, signals within the full measurement interval contribute to the equalizer used to demodulate that full measurement interval.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also