Keysight 89600 VSA .NET API
EqualizerTrainingTimeBasis Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : EqualizerTrainingTimeBasis Enumeration


Glossary Item Box

Enum values indicating the Equalizer Training time basis.

Syntax

Visual Basic (Declaration) 
Public Enum EqualizerTrainingTimeBasis 
   Inherits System.Enum
C# 
public enum EqualizerTrainingTimeBasis : System.Enum 
C++/CLI 
public enum class EqualizerTrainingTimeBasis : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
ContiguousSlotsEqualizer Training is based on the continuous slots.29.00
FrameEqualizer Training is based on the Frame.24.00
ResultLengthEqualizer Training is based on the Measurement Interval.—
SlotEqualizer Training is based on Slot.24.00
SubframeEqualizer Training is based on Subframe.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Remarks

The choice determines what portion of the signal (in time) contributes to the equalizer training procedure as used for demodulation. A subframe time basis implies the equalization used for demodulation is derived primarily from signals present in the demodulated subframe. A result length time basis assumes the equalization used for demodulation includes signals present in the entire result length of the measurement.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 23.00

See Also