Keysight 89600 VSA .NET API
IsSymbolClockOffsetCompensationEnabled Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > MeasurementExtension Class : IsSymbolClockOffsetCompensationEnabled Property


Glossary Item Box

Gets or sets a value indicating whether symbol clock offset is compensated for modulation analysis.

Syntax

Visual Basic (Declaration) 
Public Overridable Property IsSymbolClockOffsetCompensationEnabled As Boolean
C# 
public virtual bool IsSymbolClockOffsetCompensationEnabled {get; set;}
C++/CLI 
public:
virtual property bool IsSymbolClockOffsetCompensationEnabled {
   bool get();
   void set (    bool value);
}

Property Value

The default value is true.

Remarks

If true, the symbol clock error estimated for the analysis interval is applied as a compensation factor for the modulation analysis measurement. If there is clock offset between the analyzer and the transmitter of the signal to be analyzed, this will cause the clock offset to be removed and ignored by the measurement. However, if there is no clock offset, this could make the measurement slightly less accurate because the symbol clock error result used for compensation is due to noise.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 23.20

See Also