Keysight 89600 VSA .NET API
MimoEqualizerTrainingTimeBasis Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > MeasurementExtension Class : MimoEqualizerTrainingTimeBasis Property


Glossary Item Box

Gets or sets a value indicating what time basis interval is used for MIMO equalizer training.

Syntax

Visual Basic (Declaration) 
Public Overridable Property MimoEqualizerTrainingTimeBasis As EqualizerTrainingTimeBasis
C# 
public virtual EqualizerTrainingTimeBasis MimoEqualizerTrainingTimeBasis {get; set;}
C++/CLI 
public:
virtual property EqualizerTrainingTimeBasis MimoEqualizerTrainingTimeBasis {
   EqualizerTrainingTimeBasis get();
   void set (    EqualizerTrainingTimeBasis value);
}

Property Value

The default value is EqualizerTrainingTimeBasis.Frame

Remarks

When set to EqualizerTrainingTimeBasis.Slot, only signals within each demodulated slot contribute to the equalizer used to demodulation that slot. When set to EqualizerTrainingTimeBasis.ContiguousSlots, only signals within each demodulated contiguous slot region contribute to the equalizer used to demodulation that contiguous slot region. When set to EqualizerTrainingTimeBasis.Subframe, only signals within each demodulated subframe contribute to the equalizer used to demodulation that subframe. When set to EqualizerTrainingTimeBasis.Frame, only signals within each demodulated frame contribute to the equalizer used to demodulation that frame. When set to EqualizerTrainingTimeBasis.ResultLength, signals within the full measurement interval contribute to the equalizer used to demodulate that full measurement interval.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 29.40

See Also