| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property SubframeOffset As Integer | |
| C# | |
|---|---|
public abstract int SubframeOffset {get; set;} | |
Property Value
The default value is zero. The minimum value is 0 subframe and the maximum must be less than ResultLength.Valid selections will depend on the Result Length, and the Synchronization Type.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)