Keysight 89600 VSA .NET API
AntennaDetectionThreshold Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > Pdcch Class : AntennaDetectionThreshold Property


Glossary Item Box

Gets or sets a value indicating the power threshold (in dB) used for detecting whether an antenna port is active on an input channel for this PDCCH.

Syntax

Visual Basic (Declaration) 
Public Overridable Property AntennaDetectionThreshold As Double
C# 
public virtual double AntennaDetectionThreshold {get; set;}
C++/CLI 
public:
virtual property double AntennaDetectionThreshold {
   double get();
   void set (    double value);
}

Property Value

Default value is -36.0dB.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 28.60

See Also