Keysight 89600 VSA .NET API
Pdcch Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : Pdcch Class

Glossary Item Box

The following tables list the members exposed by Pdcch.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyAggregationLevelGets or sets aggregation level.  —
Public PropertyAntennaDetectionThresholdGets or sets a value indicating the power threshold (in dB) used for detecting whether an antenna port is active on an input channel for this PDCCH.  28.60
Public PropertyCandidateIndexGets or sets candidate index.  —
Public PropertyCceOffsetGets or sets the CCE offset.  24.00
Public PropertyCoresetGets the associated CORESET for this PDCCH channel  24.20
Public PropertyCRntiGets or sets a value indicating the C-RNTI for the physical channel.  28.00
Public PropertyDciFormatGets or sets the DCI Format to be used for this PDCCH physical channel.  24.00
Public PropertyDmrsPowerBoostingGets or sets a value indicating the relative power boosting of (in dB) of the DMRS associated with this physical channel.  —
Public PropertyDownlinkBwpGets the associated BWP for this PDCCH channel  24.20
Public PropertyIsDataIncludedInRmsEvmGets or sets a value indicating whether PDCCH Data is included in rmsEVM calculation/>.  24.20
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyIsDmrsIncludedInRmsEvmGets or sets a value indicating whether PDCCH Dmrs is included in rmsEVM calculation/>.  24.20
Public PropertyIsManualSetCceOffsetGets or sets a value indicating whether the CCE offset is manually set or set by CandidateIndex.  24.00
Public PropertyIsPdcchEnabledGets or sets a value indicating whether the physical channel is marked as enabled.  —
Public PropertyNameGets a value for the name for the physical channel.  —
Public PropertyPayloadSizeGets or sets payload size for PDCCH channel  —
Public PropertyPowerBoostingGets or sets a value indicating the relative power boosting (in dB) of this physical channel.  —
Public PropertyRntiGets or sets a value indicating the RNTI (used for CRC scrambling) for the physical channel.  —
Public PropertyRntiTypeGets or sets the RNTI type to be used for this PDCCH physical channel.  24.00
Public PropertySearchSpaceGets the associated search-space for this PDCCH channel  24.20
Public PropertySearchSpaceIndexGets or sets search space index.  —
Public PropertyVersionGets or sets the specification interpretation to use for PDCCH.  24.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also