Keysight 89600 VSA .NET API
CandidateIndex Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > Pdcch Class : CandidateIndex Property


Glossary Item Box

Gets or sets candidate index.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property CandidateIndex As Integer
C# 
public abstract int CandidateIndex {get; set;}
C++/CLI 
public:
abstract property int CandidateIndex {
   int get();
   void set (    int value);
}

Remarks

Default value is 0. Range is from 0 to (number of PDCCH candidates - 1).

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also