Keysight 89600 VSA .NET API
CceOffset Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > Pdcch Class : CceOffset Property


Glossary Item Box

Gets or sets the CCE offset.

Syntax

Visual Basic (Declaration) 
Public Overridable Property CceOffset As Integer
C# 
public virtual int CceOffset {get; set;}
C++/CLI 
public:
virtual property int CceOffset {
   int get();
   void set (    int value);
}

Remarks

Default value is 0. Range is from 0 to (number of CCEs - 1). when ManualSetCCEOffset is true, customer can set this value and CandidateIndex is ignored when ManualSetCCEOffset is false, this value is calculated from CandidateIndex and all the Coreset/SearchSpace configuration

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 24.00

See Also