Keysight 89600 VSA .NET API
GetResourceBlockBitmap Method
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > PdschRateMatchPattern Class : GetResourceBlockBitmap Method


Glossary Item Box

Gets a value indicating the resource block level bitmap in the frequency domain. The length of the bitmap is 275.

Syntax

Visual Basic (Declaration) 
Public MustOverride Function GetResourceBlockBitmap() As BitArray
C# 
public abstract BitArray GetResourceBlockBitmap()
C++/CLI 
public:
abstract BitArray^ GetResourceBlockBitmap(); 

Return Value

The current resource block level bitmap.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also