Keysight 89600 VSA .NET API
PdschRateMatchPattern Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : PdschRateMatchPattern Class

Glossary Item Box

The following tables list the members exposed by PdschRateMatchPattern.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyAffectedPartGets or Sets a value indicating which parts of channel are affected by this rate match pattern.  30.40
Public PropertyBwpLevelSubcarrierSpacingGets a value indicating the BWP level subcarrier spacing.  —
Public PropertyCellLevelSubcarrierSpacingGets or sets a value indicating the cell level subcarrier spacing.  —
Public PropertyEnabledGets or sets a value indicating whether a RateMatchPattern instance is enabled or not.  —
Public PropertyIdGets or sets a value indicating the ID of a RateMatchPattern.  —
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyLevelGets or sets a value indicating where a RateMatchPattern presents.  —
Public PropertyPeriodicityGets or sets a value indicating the periodicity of a RateMatchPattern in time domain.  —
Public PropertySymbolBitmapSpanGets or sets a value indicating the span of symbol bitmap.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodGetPeriodicityPatternBitmapGets a value indicating the periodicity pattern bitmap  —
Public MethodGetResourceBlockBitmapGets a value indicating the resource block level bitmap in the frequency domain. The length of the bitmap is 275.  —
Public MethodGetSymbolBitmapGets a value indicating the bitmap for symbols in a resource block in time domain.  —
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodSetPeriodicityPatternBitmapSets the periodicity pattern bitmap  —
Public MethodSetResourceBlockBitmapSets resource block level bitmap in the frequency domain. The length of the bitmap is 275.  —
Public MethodSetSymbolBitmapSets the bitmap that represents symbols in a resource block in time domain.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also