Keysight 89600 VSA .NET API
Sfi Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > Pdsch Class : Sfi Property


Glossary Item Box

Gets or sets the slot format indicator used for this PDSCH physical channel.

Syntax

Visual Basic (Declaration) 
Public Overridable Property Sfi As Integer
C# 
public virtual int Sfi {get; set;}
C++/CLI 
public:
virtual property int Sfi {
   int get();
   void set (    int value);
}

Remarks

This property helps define the set of symbols reserved for this PDSCH physical channel. This is applied in coordination with FlexibleSymbols, FirstSymbolIndex, and LastSymbolIndex.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 23.20

See Also