Keysight 89600 VSA .NET API
UserDefinedPrgSize Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > Pdsch Class : UserDefinedPrgSize Property


Glossary Item Box

Gets or sets a value indicating the user-defined precoding resource block group used by this PDSCH.

Syntax

Visual Basic (Declaration) 
Public Overridable Property UserDefinedPrgSize As Integer
C# 
public virtual int UserDefinedPrgSize {get; set;}
C++/CLI 
public:
virtual property int UserDefinedPrgSize {
   int get();
   void set (    int value);
}

Property Value

Default value is 1. Range from 1 to RBG size.

Remarks

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 25.40

See Also