Keysight 89600 VSA .NET API
Remove Method
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > PrachCollection Class : Remove Method


item
PRACH to remove from the collection

Glossary Item Box

Removes the indicated PRACH from the collection.

Syntax

Visual Basic (Declaration) 
Public MustOverride Function Remove( _
   ByVal item As Prach _
) As Boolean
C# 
public abstract bool Remove( 
   Prach item
)
C++/CLI 
public:
abstract bool Remove( 
   Prach^ item
) 

Parameters

item
PRACH to remove from the collection

Return Value

True, if the PRACH was removed from the collection.

Remarks

Note the first element in the collection cannot be removed because it is the primary PRACH.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also