Keysight 89600 VSA .NET API
PrachCollection Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : PrachCollection Class

Glossary Item Box

The following tables list the members exposed by PrachCollection.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyCountGets the number of items in the collection. (Inherited from Agilent.SA.Vsa.RemotableCollection<Prach>)—
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyItemGet the item at a specified index. (Inherited from Agilent.SA.Vsa.RemotableCollection<Prach>)—
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodClearClears the collection of items, except for the primary PRACH. The primary PRACH is the first element.  —
Public MethodCreateCreates a new PRACH channel and appends it to the collection.  —
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetEnumeratorGets an enumerator for the collection. (Inherited from Agilent.SA.Vsa.RemotableCollection<Prach>)—
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodIndexOfOverloaded. Gets the index location of the specified item within the collection. (Inherited from Agilent.SA.Vsa.RemotableCollection<Prach>)—
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodRemoveRemoves the indicated PRACH from the collection.  —
Public MethodRemoveAtRemoves the PRACH at the indicated index from the collection.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventCollectionChangedOccurs when an item is added, removed, changed, moved, or the entire list is refreshed. (Inherited from Agilent.SA.Vsa.RemotableCollection<Prach>)—
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemoteCollectionChangedOccurs when an item is added, removed, changed, moved, or the entire list is refreshed. (Inherited from Agilent.SA.Vsa.RemotableCollection<Prach>)14.00
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also