| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Function RemoveAt( _ ByVal index As Integer _ ) As Boolean | |
Parameters
- index
- Zero-based index of user to remove from the collection
Return Value
True, if the PRACH was removed from the collection.Note the first element in the collection cannot be removed because it is the primary PRACH.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)