Keysight 89600 VSA .NET API
PrachSlotIndex Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > PrachOccasion Class : PrachSlotIndex Property


Glossary Item Box

Gets or sets a value indicating the PRACH slot index within the subframe or slot for this PRACH occasion.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property PrachSlotIndex As Integer
C# 
public abstract int PrachSlotIndex {get; set;}
C++/CLI 
public:
abstract property int PrachSlotIndex {
   int get();
   void set (    int value);
}

Property Value

The default value is 0.

Remarks

For FR1, this value means the PRACH slot index within the subframes. For FR2, this value means the PRACH slot index within the slots.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also