Keysight 89600 VSA .NET API
PrachOccasion Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : PrachOccasion Class

Glossary Item Box

The following tables list the members exposed by PrachOccasion.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyEnabledGets or sets a value indicating whether this Prach Occasion is enabled or not.  —
Public PropertyFrequencyOccasionIndexGets or sets a value indicating the occasion index in frequency domain for this PRACH occasion.  —
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyOccasionIndexGets or sets a value indicating the PRACH occasion index.  —
Public PropertyPrachSlotIndexGets or sets a value indicating the PRACH slot index within the subframe or slot for this PRACH occasion.  —
Public PropertyPreambleIndexGets or sets a value indicating the preamble index of this Prach Occasion.  —
Public PropertySlotIndexGets or sets a value indicating the slot index for this PRACH occasion.  —
Public PropertySubframeIndexGets or sets a value indicating the subframe index for this PRACH occasion.  —
Public PropertyTimeOccasionIndexWithinPrachSlotGets or sets a value indicating the time occasion index within the PRACH slot for this PRACH occasion.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also