Keysight 89600 VSA .NET API
PreambleIndex Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > PrachOccasion Class : PreambleIndex Property


Glossary Item Box

Gets or sets a value indicating the preamble index of this Prach Occasion.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property PreambleIndex As Integer
C# 
public abstract int PreambleIndex {get; set;}
C++/CLI 
public:
abstract property int PreambleIndex {
   int get();
   void set (    int value);
}

Property Value

The default value is 0. Range is from 0 to 63.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also