Keysight 89600 VSA .NET API
FrequencyStart Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > Prach Class : FrequencyStart Property


Glossary Item Box

Gets or sets a value indicating the frequency start for PRACH channel.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property FrequencyStart As Integer
C# 
public abstract int FrequencyStart {get; set;}
C++/CLI 
public:
abstract property int FrequencyStart {
   int get();
   void set (    int value);
}

Property Value

The default value is 0.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also