Keysight 89600 VSA .NET API
Prach Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : Prach Class

Glossary Item Box

The following tables list the members exposed by Prach.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyBwpIdGets or sets BWP Id  24.20
Public PropertyConfigurationIndexGets or sets a value indicating PRACH configuration index.  —
Public PropertyDurationGets a value indicating the duration of PRACH channel. Duration is specified by PRACH format.  —
Public PropertyFdmGets or sets a value indicating the frequency domain occasion number for PRACH channel.  —
Public PropertyFirstSymbolIndexInSlotGets a value indicating the index of first symbol in slot.  —
Public PropertyFirstSymbolIndexInSubframeGets a value indicating the index of first symbol in subframe.  —
Public PropertyFramePeriodGets PRACH frame period  —
Public PropertyFrequencyStartGets or sets a value indicating the frequency start for PRACH channel.  —
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyIsIncludedInRmsEvmGets or sets a value indicating whether PRACH is included in rmsEVM calculation/>.  24.20
Public PropertyIsPrachEnabledGets or sets a value indicating whether the physical channel is marked as enabled.  —
Public PropertyIsR16RootSequenceIndexConfiguredGets or sets a value indicating whether prach-RootSequenceIndex-r16 is configured.  26.00
Public PropertyLraGets or sets a value indicating the LRA of the PRACH channel.  28.00
Public PropertyNcsGets a value indicating the NCS of the PRACH channel.  —
Public PropertyNumberOfPrachSlotsPerSlotGets a value indicating the number of PRACH slots in one slot.  —
Public PropertyNumberOfPrachSlotsPerSubframeGets a value indicating the number of PRACH slots in one subframe.  —
Public PropertyOccasionIndexEnabledGets or sets a value indicating whether the PRACH occasions are defined by the occasion indexes or not.  25.40
Public PropertyPowerBoostingGets or sets a value indicating the relative power boosting (in dB) of this physical channel.  —
Public PropertyPrachFormatGets PRACH preamble format  —
Public PropertyPrachOccasionsGets a reference to the collection of PRACH occasion settings.  25.40
Public PropertyR16RootSequenceIndexGets or sets a value indicating the prach-RootSequenceIndex-r16 for this physical channel.  26.00
Public PropertyRestrictedSetGets or sets a value indicating the restricted set for PRACH channel.  —
Public PropertyRootSequenceIndexGets or sets a value indicating the root sequence index on this physical channel.  —
Public PropertySpectrumTypeGets or sets a value indicating PRACH spectrum type.  —
Public PropertySubcarrierSpacingGets or sets a value indicating the subcarrier spacing for this PRACH channel.  —
Public PropertyTimeOccasionsPerPrachSlotGets a value indicating the number of time occasions per PRACH slot.  —
Public PropertyZeroCorrelationZoneConfigurationGets or sets a value indicating the zero correlation zone configuration on this physical channel.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetFrameOffsetsGets frame offsets.  —
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodGetPrachSlotIndexesGets PRACH slot indexes.  —
Public MethodGetSubframeIndexesGets subframe indexes.  —
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also