| Visual Basic (Declaration) | |
|---|---|
Public Overridable Property InterlaceOneIndex As Integer | |
| C# | |
|---|---|
public virtual int InterlaceOneIndex {get; set;} | |
Property Value
Default value is 0. For numerology 15kHz, the minimum value is 0, the maximum value is 9. For numerology 30kHz, the minimum value is 0, the maximum value is 4This property corresponds to the higher-layer parameter interlace1-r16 in PUCCH-format2-r16 or PUCCH-format3-r16 information element. Multiple interlaces are defined for numerology 15kHz and 30kHz . For Numerology 15kHz, 10 interlaces are defined. For Numerology 30kHz, 5 interlaces are defined. When InterlacedTransmissionEnabled is true, for PUCCH format 2 and 3, besides InterlaceZeroIndex, it can be configured with a second interlace for transmission. This value indicates the index of the second interlace on which the PUCCH is allocated.This value is only used when InterlaceOneConfigured is true.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 25.20