| Visual Basic (Declaration) | |
|---|---|
Public Overridable Property RbSetIndexForInterlace As Integer | |
| C# | |
|---|---|
public virtual int RbSetIndexForInterlace {get; set;} | |
Property Value
Default value is 0, the minimum value is 0, the maximum value is 4.This property corresponds to the higher-layer parameter
rb-SetIndex in PUCCH-Resource-r16 information element. When New Radio carrier is in unlicensed spectrum, it is possible some segments of the spectrum are not available for New Radio signal transmission, and these segments are defined as Intra-Cell guard bands. These guard bands divide the whole carrier into several RB sets, at most there can be 4 guard bands and 5 RB sets. When the PUCCH uses interlaced transmission, this value indicates the index of the RB set on which this PUCCH is allocated. , ,Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 25.20