Keysight 89600 VSA .NET API
CellLevelSubcarrierSpacing Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > PuschRateMatchPattern Class : CellLevelSubcarrierSpacing Property


Glossary Item Box

Gets or sets a value indicating the cell level subcarrier spacing.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property CellLevelSubcarrierSpacing As RateMatchPatternSubcarrierSpacing
C# 
public abstract RateMatchPatternSubcarrierSpacing CellLevelSubcarrierSpacing {get; set;}
C++/CLI 
public:
abstract property RateMatchPatternSubcarrierSpacing CellLevelSubcarrierSpacing {
   RateMatchPatternSubcarrierSpacing get();
   void set (    RateMatchPatternSubcarrierSpacing value);
}

Remarks

This property is applicable for cell level rate matching pattern only. The value 15 kHz corresponds to µ=0, the value 30 kHz corresponds to µ=1, and so on. Only the values 15 kHz, 30 kHz or 60 kHz (FR1), and 60 kHz or 120 kHz (FR2) are applicable (see TS 38.214 [19], clause 5.1.4.1).

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also