Keysight 89600 VSA .NET API
AntennaPortsUsed Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > Pusch Class : AntennaPortsUsed Property


Glossary Item Box

Gets or sets a value indicating the PUSCH antenna ports used by this PUSCH.

Syntax

Visual Basic (Declaration) 
Public Overridable Property AntennaPortsUsed As Integer
C# 
public virtual int AntennaPortsUsed {get; set;}
C++/CLI 
public:
virtual property int AntennaPortsUsed {
   int get();
   void set (    int value);
}

Property Value

Default value is 1. Range of value is 1(antenna port 0 is active) to 63(all 8 antenna ports are active).

Remarks

when UseAntennaPortsIndex is true, this value is calculated based on AntennaPortsIndex, DmrsConfigType, IsMimoPrecodingOn, DmrsMaxLength, RankNumber when UseAntennaPortsIndex is false, customer can set the 8 DMRS ports active status through the 8 bits, each bit indicating each DMRS port is active or not, LSB means antenna port 0, etc.. Refer to 7.3.1.1.2 of 38.212 for more details. The number of DMRS ports is the layer number of this PUSCH.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 23.20

See Also