Keysight 89600 VSA .NET API
DmrsDuration Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > Pusch Class : DmrsDuration Property


Glossary Item Box

Gets or sets a value indicating the PUSCH DMRS duration.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property DmrsDuration As DmrsDuration
C# 
public abstract DmrsDuration DmrsDuration {get; set;}
C++/CLI 
public:
abstract property DmrsDuration DmrsDuration {
   DmrsDuration get();
   void set (    DmrsDuration value);
}

Property Value

Default value is DmrsDuration.SingleSymbol.

Remarks

The PUSCH DMRS duration can be 1 symbol or two symbols, it is limited by the DmrsMaxLength

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also