| Visual Basic (Declaration) | |
|---|---|
Public Overridable Property NumberOfAntennaPorts As NumberOfAntennaPorts | |
| C# | |
|---|---|
public virtual NumberOfAntennaPorts NumberOfAntennaPorts {get; set;} | |
| C++/CLI | |
|---|---|
public: virtual property NumberOfAntennaPorts NumberOfAntennaPorts { NumberOfAntennaPorts get(); void set ( NumberOfAntennaPorts value); } | |
Property Value
Default value is NumberOfAntennaPorts.One.When this PUSCH is codebook-based transmission, both the PUSCH data part and its DMRS are precoded using a predefined matrix. The precoding matrices are defined in section 6.3.1.5 of 3GPP 38.211. The following three parameters decides which precoding matrix is used for this PUSCH: 1) Layer number(also DMRS port number), we use AntennaPortsIndex or AntennaPortsUsed to define which DMRS ports are used, and the number of DMRS ports used is the layer number. 2) Number of antenna ports, which is this parameter. 3) Precoding Matrix index, PrecodingMatrixIndex
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 27.0