Keysight 89600 VSA .NET API
AntennaGroupNumber Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > RectangularAntennaPanelArray Class : AntennaGroupNumber Property


Glossary Item Box

Gets or sets the number of antenna group in this antenna array.

Syntax

Visual Basic (Declaration) 
Public Property AntennaGroupNumber As Integer
C# 
public int AntennaGroupNumber {get; set;}
C++/CLI 
public:
property int AntennaGroupNumber {
   int get();
   void set (    int value);
}

Remarks

When there are multiple antenna groups in this antenna array, it means all these antenna groups have the same antenna array layout. For example, if the antenna array has two polarizations overlapped with each other, the antenna group number is 2.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 27.00

See Also