Keysight 89600 VSA .NET API
RectangularAntennaPanelArray Class Members
See Also  Properties  Methods 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : RectangularAntennaPanelArray Class

Glossary Item Box

The following tables list the members exposed by RectangularAntennaPanelArray.

Public Constructors

 NameDescriptionMinimum SW Version
Public ConstructorRectangularAntennaPanelArray ConstructorOverloaded.   —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyAntennaCenterFrequencyGets or sets the frequency used to define the element spacing if the ElementSpacingUnit is ElementSpacingUnit.WaveLength.  27.00
Public PropertyAntennaGroupNumberGets or sets the number of antenna group in this antenna array.  27.00
Public PropertyElementNumberPerPanelInHorizontalDirectionGets or sets the number of antenna elements in an antenna panel in the horizontal direction.  27.00
Public PropertyElementNumberPerPanelInVerticalDirectionGets or sets the number of antenna elements in an antenna panel in the vertical direction.  27.00
Public PropertyElementSpacingInHorizontalDirectionGets or sets the distance between the adjacent elements within the same antenna panel in the horizontal direction.  27.00
Public PropertyElementSpacingInVerticalDirectionGets or sets the distance between the adjacent elements within the same antenna panel in the vertical direction.  27.00
Public PropertyElementSpacingUnitGets or sets the unit of PanelSpacingInHorizontalDirection, PanelSpacingInVerticalDirection, ElementSpacingInHorizontalDirection, ElementSpacingInVerticalDirection.  27.00
Public PropertyPanelNumberPerGroupInHorizontalDirectionGets or sets the number of antenna panels in an antenna group in the vertical direction.  27.00
Public PropertyPanelNumberPerGroupInVerticalDirectionGets or sets the number of antenna panels in an antenna group in the vertical direction.  27.00
Public PropertyPanelSpacingInHorizontalDirectionGets or sets the distance between the adjacent panels in the horizontal direction.  27.00
Public PropertyPanelSpacingInVerticalDirectionGets or sets the distance between the adjacent panels in the vertical direction.  27.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodSerialize  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also