Keysight 89600 VSA .NET API
ElementNumberPerPanelInHorizontalDirection Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > RectangularAntennaPanelArray Class : ElementNumberPerPanelInHorizontalDirection Property


Glossary Item Box

Gets or sets the number of antenna elements in an antenna panel in the horizontal direction.

Syntax

Visual Basic (Declaration) 
Public Property ElementNumberPerPanelInHorizontalDirection As Integer
C# 
public int ElementNumberPerPanelInHorizontalDirection {get; set;}
C++/CLI 
public:
property int ElementNumberPerPanelInHorizontalDirection {
   int get();
   void set (    int value);
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 27.00

See Also