Keysight 89600 VSA .NET API
ElementSpacingInHorizontalDirection Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > RectangularAntennaPanelArray Class : ElementSpacingInHorizontalDirection Property


Glossary Item Box

Gets or sets the distance between the adjacent elements within the same antenna panel in the horizontal direction.

Syntax

Visual Basic (Declaration) 
Public Property ElementSpacingInHorizontalDirection As Double
C# 
public double ElementSpacingInHorizontalDirection {get; set;}
C++/CLI 
public:
property double ElementSpacingInHorizontalDirection {
   double get();
   void set (    double value);
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 27.00

See Also